Salesforce

ArcFM Solution Maps and Apps - Communications

« Go Back
Information

 

NameDescriptionLinks 

Aggressive Dogs

Field personnel can use the Aggressive Dogs webmap to add and view aggressive dog features in the field to identify and warn of areas where aggressive dogs are located in their service territories.

 

Your organization, third party contractors, or the general public can use ArcGIS Online to access the Aggressive Dogs webmap.

Try it!


Download (requires login):
Aggressive Dogs

Gray-Scale Maps

The Gray-Scale Maps webmap provides users with a simple-to-configure map that is optimized for gray-scale printing. Utility assets and landbase information are displayed in a monochrome display while still providing the users with an intuitive map.

Try it!


Download (requires login):
Grayscale maps for printing

Mobile Map Services

Mobile crews for electric, gas & water, and communication organizations can use Mobile Map Services to view information from either ArcFM Mobile or Esri’s ArcGIS Online in the field, publishing operational maps used for viewing or mobile work in either online or offline mode.

 

Your organization, third-party contractors, or the general public can use ArcGIS Online to access the Mobile Map Services webmap.

Try it! - Coming soon


Download (requires login):
Mobile Map Services

Joint-Use Inventory

Use the Joint-Use Inventory template to quickly view which poles and other support structures have joint-use attachments, as well as the type of each attachment, in the current database. The symbology is set so that if a pole has multiple attachments, the X will appear as an asterisk (*) with arms of different colors based on the attachment type.


This kit also contains a Joint-Use Field Notes template you can use to create a field note feature to capture any changes and edits from field crews and visualize where they have made those notes.


Your organization, third-party contractors, or the general public can use ArcGIS Online to access both the Joint-Use Inventory and Joint-Use Field Notes webmaps.

Try it!


Download (requires login):
Joint-Use Inventory

Police Escort Area

Field personnel can use the Police Escort Area webmap to highlight, edit, and view all neighborhoods where police escorts are required in their service area.

 

Your organization, third-party contractors, or the general public can use ArcGIS Online to access the Police Escort Area webmap. You can control who gets access through ArcGIS Online.

Try it!


Download (requires login):
Police Escort Area

Fiber Facilities

The Fiber Facilities map enables utility staff, from field technicians to customer service representatives, access to basic geographic utility information. This core fiber optic map is designed to make asset information accessible to the organization using a web browser or native client.

 

The Fiber Facilities map can be deployed in Portal for ArcGIS or within an ArcGIS Online organizational account.

Try it!


Download (requires login):
Fiber Facilities

Fiber Availability

The Fiber Availability map provides utility staff, from field technicians to customer service representatives, access to basic geographic utility information. This core fiber optic utility map makes availability information accessible to the organization using a web browser or native client.

 

Deploy the Fiber Availability map in Portal for ArcGIS or within an ArcGIS Online organizational account.

Try it!


Download (requires login):
Fiber Availability

 

Additional Information
ArcFM Solution Maps and Apps - Communications
_
ArcFM-Solution-Maps-and-Apps-Communications
Knowledge
Published
 

Powered by