Salesforce

Customer Outage Portal

« Go Back
Information

Overview

 

The Customer Outage Portal is a web-based application that allows utility customers to view current incidents in Responder, including detailed information about those incidents. The Customer Outage Portal also provides an example of how you can allow customers to report an outage through the application.

 

The Customer Outage Portal can be deployed in Portal for ArcGIS or within an ArcGIS Online organizational account. The application consists of:

  • An outage feature service {can be published using the sample file geodatabase and mxd file installed as part of the MSI - Located by default in C:\Program Files (x86)\Miner and Miner\Sample Data}
  • An outage map {created based on the outage feature service}
  • An application built with WebApp Builder hosted in ArcGIS Online

 

 

Requirements

 

The Customer Outage Portal requires specific technical experience and software.

 

RequirementDescription
Experience
  • Publishing GIS Services
  • Authoring maps
  • Administering groups and organizing content in an ArcGIS organization
  • Configuring ArcGIS Online or Portal for ArcGIS configurable application templates
  • Knowledge to publish map services securely outside the corporate firewall
  • Configuring Schneider Electric’s Responder product
Software
  • Schneider Electric’s Customer Outage Portal
  • Schneider Electric’s Responder product version 10.2.1c, 10.2.1d, 10.6.1, 10.6.1a, 10.6.1b, 10.8.1 (different versions of the app exist for 10.2, 10.6, and 10.8))
  • ArcGIS for Desktop 10.2.1 OR 10.6.1 OR 10.8.1 (different versions of the app exist for 10.2, 10.6, and 10.8)
  • ArcGIS for Server 10.1-10.8.1 (Standard or Advanced)
  • Enterprise Database
  • .NET Framework 4.6.1 or greater
  • Other requirements, which follow those for the versions of the SE Responder product being used with the Customer Outage Portal, are located here.
Applications
  • Customer Outage Portal (ArcGIS configurable web application)

 

 

Zip File Contents

 

SEGeospatialOutageMap.msi – A Microsoft installer file containing everything needed to install the windows service, map, and application.

 

 

Documentation

 

Customer Outage Portal Configuration

 

Try Now

 

Outage Map

 

 

All Maps and Apps by Industry

ArcFM Solution Maps and Apps - Electric

ArcFM Solution Maps and Apps - Gas/Water

ArcFM Solution Maps and Apps - Communications


SEGeospatialOutageMap.zip - 10.2.1 - V5
SEGeospatialOutageMap.zip - 10.6.1 - V4
SEGeospatialOutageMap.zip - 10.8.1 - V2

Additional Information
Customer Outage Portal
Shawn Leingang
Customer-Outage-Portal
Knowledge
Published
 

Powered by