Salesforce

Outage History

« Go Back
Information

Overview

 

Playback an outage with the Outage History template. The map is a time-aware spatial representation that displays how the outage fanned out across the service territory. Visible information includes impacted customers and which of those users called to report an outage. Use the Time slider widget to play, pause and traverse back and forth in time, to visualize the impact to various areas during the outage or storm period.

 

Requirements

 

The Outage History map requires specific technical experience and software.

 

RequirementDescription
Experience
  • Publishing GIS Services
  • Authoring maps
  • Working with ArcMap Query layers (SQL) and Time slider tool
  • Administering groups and organizing content in an ArcGIS organization
  • Configuring ArcGIS Online or Portal for ArcGIS configurable application templates
  • Knowledge to publish map services securely outside the corporate firewall
Software
  • ArcGIS for Desktop 10.1-10.4 (Standard or Advanced)
  • ArcGIS for Server  10.1-10.4 (standard or Advanced)
  • Enterprise Geodatabase
    • For Oracle databases that use SDEBINARY as the spatial data type, please contact Neil Batchelor.  You will need to use SDE Command Line tools to generate the appropriate tables
Applications
  • Basic Viewer (ArcGIS configurable web application template)
Data
  • Map data with date/Time fields, for use with the time slider based visualization

 

Zip File Contents

  • RX_Customers_and_loadpoints.mxd – A map document that includes customer calls (from IVR) and outage location (load points) query layers, with symbology, to be used for publishing the map service to ArcGIS Server.
  • OutageHistory.png – Icon to use with the application that you will create.
  • Rx_query_layer_SQL.txt – Contains the raw sql used to build the ArcMap Query layers.
  • OutageHistory-GettingStarted.docx – Instructions to start the process of using this Playback Outage template.
  • OutageHistory-Home.docx – This document.

 

Try Now

Playback Outage

 

All Maps and Apps by Industry

Electric

Gas/Water

Communications


outagehistory.zip

Additional Information
Outage History
_
Outage-History
Knowledge
Published
 

Powered by