Salesforce

Sample - Feeder Label Text

« Go Back
Information
Versions: 10.2.1a - current
Product Availability: ArcFM with Feeder Manager 2.0
 
This project sample shows how to change feature labels that are part of a Feeder Manager 2.0 geometric network whenever ArcFM emits a feeder change event. This sample updates the LabelText attribute of overhead conductor features to reflect the current feeder id and energized phases.
 
How to implement:
  1. Open FeederLabelText.sln and connect any broken references.     
  2. Build the solution.
  3. Ensure the FeederLabelText.dll has been built into the project's \obj\Debug folder.
  4. Copy the FeederLabelText.dll into your Miner and Miner\FeederManager directory. Create the FeederManager (one word, Pascal case) folder if it does not already exist.
  5. Open ArcMap with an electric geometric dataset.
  6. Locate an overhead conductor.
  7. Make changes to the network that impact the conductor's feeder information (e.g., open or close a fuse).
  8. Notice the conductor's label text changes on a feeder change event.
 
Requires:
All of the files shown below are required for the project to build successfully.
FileDescription
FeederLabelText.slnVisual Studio Solution file.
FeederLabelText.csprojC# project file.
UpdateFeederLabelText.csClass module for the autoupdater.


FeederLabelText.zip
Additional Information
Sample - Feeder Label Text
_
Sample-Feeder-Label-Text
Knowledge
Published
 

Powered by