EXI-13325 - eliminate e_sqlite3.dll security vulnerability CVE-2023-7104 by upgrading to the latest SQLitePCLRaw nuget package (2.1.7).
EXI-13352 - Build Commit Getting Appended Causing Auto-update to Not Work Note: If you applied patch 2.0.3, you will need to manually apply this patch. Note: Please see the note from the 9/20 patch, as those notes still apply here.
EXI-12125 - Component Info - On Initial Zoom, Toast Is Displayed if Settings Don't Exist
EXI-12030 - ArcFM UN Changing Network Categories for Connected Units
Note: With this latest Editor XI 11.5.2 hotfix, we have updated our tooling to expect the latest Network Categories (additions of E:Has Connected Units, E:Has Disconnected Units, and E:Has Conductor Info, as well as the removal of E:Has Units). Please refer to the latest version of the Whitepaper for the most up to date Network Category expectations.
EXI-2256 - The PhasesCurrent attribute that used to control both phases allowed through and phases present has been changed to PhasesPassedThrough, and a field called PhasesPresent has been added as well. This fixes issues where we couldn't differentiate which features are NOT tap features and which inherently didn't restrict network flow by phase.
EXI-3888 - Handle task was canceled exceptions under load
EXI-3981 - Fix crash during validation
EXI-4143 - Ensure version gets deleted when session doesn't get created due to service not responding
EXI-4144 - Provide better error message when session fails to be created
EXI-4154 - Remove message about nothing being found after removing filters
EXI-4178 - Save Edits dialog will now show if switching versions with pending edits
EXI-4555 - Clear out existing validation when switching versions
EXI-4748 - Enforce only one session being created per markup
EXI-5090 - Fix token refresh issues
EXI-5269 - Handle lowercase tenant IDs
EXI-5368 - Workaround for failed validation
EXI-5370 - Fix object reference error in Session Manager
EXI-2497 - User Agent fails to refresh its token successfully for EXI after 24 hours of running
EXI-2903 - EXI Shouldn't Allow Multiple Domain Networks Within The Same Utility Type
EXI-2974 - Validation Assistant needs to perform a spatial query to determine if there are dirty areas/errors in the extent for Enterprise 10.8
EXI-3065 - A null reference exception can occur if the user tries to show all markups on a null map
EXI-3069 - A crash can occur if an unhandled task canceled exception happens when showing all markups
EXI-3070 - Update Messaging and Workflow Surrounding Version Mismatch Between Add-ins
EXI-3177 - Limit Size of Listview Items and Session Card Height With Long Descriptions
Resolved Issues - 11.2 - 3/6/20 Release (1.4.0)
EXI-2524 - Flow Direction doesn't respect map rotation.
EXI-2511 - Certain data won't trace in EXI.
EXI-2703 - If kv storage service is down, session manager fails to create edit assignments.
EXI-2197 - The progress spinner that runs during trace execution keeps running after results are returned until the mouse is moved.
EXI-2303 - A timeout occurs when creating a session that happens most often when ArcGIS Pro first opens.
EXI-2779 - Reassign button won't enable with only two users in the group.
Resolved Issues - 11.1.1 2/18/2020 Patch (1.3.3)
EXI-2689 - Attempting to perform a trace on a point feature without a terminal configuration fails on Pro 2.5 - NOTE: This adds ArcGIS Pro 2.5 support to 11.1.1, but it precludes using ArcGIS Pro 2.4 from this release forward.
Resolved Issues - 11.1.1 1/14/2020 Patch (1.3.2)
EXI-2505 - Valve Component Info does not work in UPDM 2019
EXI-2425 - The Redline dockpane should check if a redline is part of a session within the 'Create Session' function
EXI-2378 - A certain data condition causes find feeder to crash because it cannot find the source of the subnetwork
EXI-2428 - Isolation Trace fails to execute in UPDM
EXI-2379 - Unable to complete redline sessions in ArcGIS Pro
EXI-2380 - If an operational map does not exist but there is a GUID for one in a Redline type document, EXI crashes when showing all redlines.
EXI-2431 - A crash occurs while trying to read domain networks in the UN Wrapper.
EXI-2382 - Enhancement - Resolve conflicting assembly between Editor XI and any other installed Add-in within ArcGIS Pro
Resolved Issues - 11.1.1 11/25/2019 Patch (1.3.1)
EXI-2259 - System error when ArcFM Redlining attempts to add layer to the map that can't be found
EXI-2260 - Resourcing layers to a UN feature service that does not have a configuration in solution center leads to many error toast messages
EXI-2262 - Redlines associated with sessions are not being filtered out from the Redline Dockpane
EXI-2263 - Properly catch all task canceled exceptions
EXI-2266 - Error when adding a redline to a session that is now closed
EXI-2300 - Issues With Session Manager drop down getting out of date
Resolved Issues - 11.1.1- 10/2/19 Release (1.3.0)
Surface Area and Total Length summaries are not calculated correctly for Gas data despite correct calculations in Electric data (EXI-1396 - fixed in Pro 2.4).
Custom Construction tools (Phase Assign) ignore Utility Network rules based snapping – (Esri BUG-000116943 - fixed in Pro 2.4) Custom construction tools allow for the snapping of features that don’t have mutual rules in the Rules table leading to validation errors that the rules based snapping wouldn’t have allowed.
Subnet Line summaries are not consistent when compared with a calculation of the fields – (ArcGIS Enterprise Bug - BUG-000114245 - fixed in Pro 2.3) The network management tool is given false information in regard to the summaries that are configured on the subnetline using Esri tooling for gas data.
EXI-1291 - When Map and Feature Services are shared to Everyone, we are not able to create versions through the REST API even though there are valid credentials tied to the request
EXI-1606 - Object ID information removed information from ArcFM Search Results and replaced with Primary Display Field.
EXI-2074 - Graphical tracing does not respect true curves.
EXI-2090 - Isolation trace results are different than expected.
EXI-2190 - Changing versions with ArcFM Editor XI installed causes an error message.