Entries in italics are supported but not certified. Uncertified environments are given full normal support, and any issues found to be caused by incompatibility with the uncertified software will be evaluated for resolution.
Hardware requirements for Editor XI follow those for Esri's ArcGIS Pro, which can be found here.
Please note that while ArcFM Editor requires a specific version of ArcGIS Pro, it also requires a specific version of ArcSDE per Esri help documentation. We will support, to the best of our ability, combinations of versions that do not match, but doing so is not recommended, and we will not provide patches to our software to support such combinations.
Service packs and patches for operating systems and database management systems already listed as supported or certified in the charts below are automatically considered supported, but not certified, unless noted otherwise.
General Availability support is denoted by (GA) in the header. See ArcFM XI Series Product Life Cycle Support Policy for more details.
SE makes efforts to support new releases of Esri software (ArcGIS Pro, ArcGIS Enterprise, UN Versions) within 1-2 months of their release on current GA versions. This can depend on the size of changes Esri made and if problems are found in certification testing. SE will post information about their support as soon as it is available.
Note that older versions of Editor XI can be referenced here: ArcFM Editor XI Supported Versions Archive.
Editor XI Add-in Version | 11.4.2 | 11.5 | 11.5.1 | 11.5.2 (GA) | 2024 C1 (GA) | 2025 C1 (GA) | Notes |
---|
ArcGIS Pro Versions | 2.9 | 2.9 | 2.9 |
3.1 3.3
|
3.1 3.3
|
3.3
|
See the ArcGIS Pro system requirements .
Pro/Enterprise/UN supported combinations can be referenced at this link and follow the Network Management Release Plan from Esri.
See above the table for a statement on SE's planned support for future Esri releases
|
---|
ArcGIS Enterprise Versions | 10.8.1 10.9.1 | 10.8.1 10.9.1 | 10.8.1 10.9.1 | 10.9.1 11.1 | 11.1 11.3 | 11.1 11.3 |
ArcFM Editor add-in installs on top of ArcGIS Pro. ArcGIS Enterprise is used for the services that ArcGIS Pro accesses.
Pro/Enterprise/UN supported combinations can be referenced at this link.
See above the table for a statement on SE's planned support for future Esri releases
|
---|
ArcFM Autoupdater Framework | N/A | N/A | N/A | N/A |
2.0.2 3.0.0 4.0.0
| 3.0.0 4.0.0 | |
---|
ArcGIS Products | ArcGIS Pro ArcGIS Enterprise | Same as last release | Same as last release | Same as last release | Same as last release | Same as last release | |
---|
ArcGIS Licensing | Standard or Greater | Standard or Greater | Standard or Greater | Standard or Greater | Standard or Greater | Standard or Greater | This applies to both ArcGIS Pro and Enterprise. |
---|
ArcFM Licensing | ArcFM Editor | ArcFM Editor | ArcFM Editor | ArcFM Editor | ArcFM Editor | ArcFM Editor | License is provided through Tenant Provision |
---|
UN Model Version | v4 v5 | v4 v5 | v4 v5 | v4 v5 v6 | v4 v5 v6 | v4 v5 v6 |
See the Utility Network requirements
Pro/Enterprise/UN supported combinations can be referenced at this link .
Note that Named Trace functionality requires v5
Note you must be on Enterprise 11.1 or later to use v6
See above the table for a statement on SE's planned support for future Esri releases
|
---|
UN Tools | 2.9 | 2.9 | 2.9 | 2.9 | 2.9 3.1 | 2.9 3.1 3.3 | This is only applicable to what version should be used with our Sample Data. Otherwise, this is a set of esri tools that doesn't relate to Editor XI. |
---|
Desktop Operating System | Windows 10 | Windows 10 | Windows 10 | Windows 10 Windows 11 | Windows 10 Windows 11 | Windows 10 Windows 11 | All Operating Systems mentioned are 64-bit
Note that we will always support the latest version of Windows 11 released by Microsoft unless stated otherwise. |
---|
Server Operating System | Windows Server 2012 R2 Windows Server 2016 Windows Server 2019 | Same as last release | Same as last release | Same as last release | Same as last release | Same as last release | All Operating Systems mentioned are 64-bit
Note that we will always support the latest version of Windows Server 2019 released by Microsoft unless stated otherwise. |
---|
Virtual Environments | Supported | Supported | Supported | Supported | Supported | Supported | |
---|
.NET Desktop Runtime | 4.8 | 4.8 | 4.8 |
.NET 6 .NET 8
| .NET 6 .NET 8 | .NET 8 | Dependent on ArcGIS Pro Version |
---|
RDBMS | Oracle SQL Server PostgreSQL SAP HANA | Same as last release | Same as last release | Same as last release | Same as last release | Same as last release | We are RDBMS agnostic and support whatever Esri does from an ArcGIS Pro perspective. Note that Oracle Spatial (SDO) and ST Geometry with Branch Versioning are supported. Note that FGDB is not supported at this time. |
---|
ArcFM UN Asset Package | | | | | • ArcFM Balanced AP v1.2 • ArcFM Unbalanced AP v1.2 | • ArcFM Balanced AP v1.2 • ArcFM Unbalanced AP v1.2 | |
---|
ArcFM Autoupdater XI
ArcFM Autoupdater XI Framework Version
| 2.0.2 | 3.0.0 | 4.0.0 | Notes |
ArcFM Editor XI Version |
2024 C1 2024 C1 SP1
|
2024 C1 2024 C1 SP1 2025 C1
| 2024 C1 2024 C1 SP1 2025 C1 | |
ArcGIS Pro Versions | ALL | ALL | ALL | Since the SOI run on the server, the version of ArcGIS Pro should not matter. Until otherwise noted all version of ArcGIS Pro are supported. |
ArcGIS Enterprise Versions | 11.1 | 11.1 11.3 | 11.3 | |
.NET Desktop Runtime | .NET 6 | .NET 6 | .NET 8 | This is the version that the SOI framework was compiled against. Not the required version. The targeted runtime version will depend on the version of ArcGIS Enterprise. |