Salesforce

ArcFM Editor XI Supported Versions Archive

« Go Back
Information

This document is an archive of Supported Versions information for old releases of ArcFM Editor XI.  For more recent and currently supported releases, please see ArcFM Editor XI Supported Versions.

 

ArcFM Editor XI Older Versions

 11.0 (Patch 1.0.0.9)11.0.111.111.1.111.211.2.111.311.411.4.1Notes
ArcGIS Pro Versions2.22.2.3
2.2.4
2.3
2.4
2.4
2.5
2.5
2.6
2.5
2.6
2.7
2.6
2.7
2.8
2.9
2.92.9Note for 11.1.1 users:  ArcGIS Pro version 2.4 is only supported through build 1.3.2 (January Patch).  Starting at build 1.3.3 (February Patch), we added support for ArcGIS Pro 2.5 and ONLY support this version.
ArcGIS Enterprise Versions10.6.110.6.110.7
10.7.1
Same as last release10.7.1
10.8
10.8.1
Same as last release10.7.1
10.8
10.8.1
10.9
10.9.1
10.9.110.9.1ArcFM Editor add-in installs on top of ArcGIS Pro.

ArcGIS Enterprise is used for the services that ArcGIS Pro accesses.
ArcGIS ProductsArcGIS Pro
ArcGIS Enterprise
Same as last releaseSame as last releaseSame as last releaseSame as last releaseSame as last releaseSame as last releaseSame as last releaseSame as last release 
ArcGIS LicensingStandard or GreaterStandard or GreaterStandard or GreaterStandard or GreaterStandard or GreaterStandard or GreaterStandard or GreaterStandard or GreaterStandard or GreaterThis applies to both ArcGIS Pro and Enterprise.
ArcFM LicensingArcFM EditorArcFM EditorArcFM EditorArcFM EditorArcFM EditorArcFM EditorArcFM EditorArcFM EditorArcFM EditorLicense is provided through Tenant Provision
UN Model Version   v3v3v3
v4
v4
v5
v4
v5
v4
v5
Conduit Manager is only supported on UN v4 (or later) Electric
UN Tools2.2.1.22.2.1.22.3
2.4.x
2.4.x2.5.x2.6.x2.6.x or later2.92.9This is only applicable to what version should be used with our Sample Data.  Otherwise, this is a set of esri tools that doesn't relate to Editor XI.
Desktop Operating SystemWindows 7
Windows 10
Same as last releaseSame as last releaseSame as last releaseWindows 10Windows 10Windows 10Windows 10Windows 10All Operating Systems mentioned are 64-bit

Note that we will always support the latest version of Windows 10 released by Microsoft unless stated otherwise.
Server Operating SystemWindows Server 2012 R2 Windows Server 2012 R2
Windows Server 2016
Windows Server 2012 R2
Windows Server 2016
Windows Server 2019
Same as last releaseWindows Server 2012 R2
Windows Server 2016 
Windows Server 2019
Same as last releaseWindows Server 2012 R2
Windows Server 2016 
Windows Server 2019
Same as last releaseSame as last releaseAll Operating Systems mentioned are 64-bit

Note that we will always support the latest version of Windows Server 2019 released by Microsoft unless stated otherwise.
Virtual EnvironmentsSupportedSupportedSupportedSupportedSupportedSupportedSupportedSupportedSupported 
.NET Framework4.6.24.6.24.6.24.6.24.84.84.84.84.8 
RDBMSOracle
SQL Server
Oracle
SQL Server
PostgreSQL
SAP HANA
Same as last releaseSame as last releaseSame as last releaseSame as last releaseSame as last releaseSame as last releaseSame as last releaseWe are RDBMS agnostic and support whatever Esri does from an ArcGIS Pro perspective.   
Note that FGDB is not supported at this time.

 

Additional Information
ArcFM Editor XI Supported Versions Archive
Nick Wanke
Editor-XI-Supported-Versions-Archive
Knowledge
Published
 

Powered by